21.6.8 GENERATEPROGRAMMINGDATA

Description

"GENERATEPROGRAMMINGDATA" is the name of a command tool used in the run_tool command. The "run_tool -name {GENERATEPROGRAMMINGDATA}" Tcl command generates the files needed for generating programming bitstream files.

run_tool -name {GENERATEPROGRAMMINGDATA}

Arguments

ParameterTypeDescription
NoneNoneNone
Return TypeDescription
IntegerReturns 0 on success and 1 on failure.

Error Codes

Error CodeDescription
NoneNone

Supported Families

Supported Families
PolarFire®
PolarFire SoC
RTG4
SmartFusion® 2
IGLOO® 2

Example

The following command generats programming bitstream file:

run_tool -name {GENERATEPROGRAMMINGDATA}