21.6.24 VERIFYPOWER

Description

"VERIFYPOWER" is a command tool used in run_tool. The command run_tool passes an absolute path of the script file that contains power-specific Tcl commands to the "VERIFYPOWER" command and executes it.

run_tool -name {VERIFYPOWER} -script {power_analysis.tcl}

Arguments

ParameterTypeDescription
scriptstringSpecify absolute path of the script file. This is an optional parameter. Script contains power-specific Tcl commands.
Note: You can include power-specific Tcl commands to generate power reports.
Return TypeDescription
IntegerReturns 0 on success and 1 on failure.

Error Codes

Error CodeDescription
NoneNone

Supported Families

Supported Families
PolarFire®
PolarFire SoC
RTG4
SmartFusion® 2
IGLOO® 2

Example

The following example changes SmartPower operating condition settings from the default to 40 °C junction temperature and 1.25V VDD.

# Change from pre-defined temperature and voltage mode (COM,IND,MIL) to SmartPower custom
smartpower_set_temperature_opcond -use "design" 
smartpower_set_voltage_opcond -voltage "VDD" -use "design"

# Set the custom temperature to 40C ambient temperature.
smartpower_temperature_opcond_set_design_wide -typical 40 \
                                              -best 40 \
                                              -worst 40
# Set the custom voltage to 1.25V
smartpower_voltage_opcond_set_design_wide -voltage "VDD" \
                                          -typical 0.970 \
		                          -best 1.25 -worst 1.25