Description
This is the FlashPro-specific tcl command that pings one or more programmers. Right-click a programmer and choose Ping.
Note: You can click the Refresh/Rescan for Programmers button to quickly ping new programmers.
ping_prg -name {name}
Arguments
Parameter | Type | Description |
---|
name | string | Specifies the programmer to be pinged. Repeat this argument for multiple programmers. See example below. This is mandatory. |
Return Type | Description |
---|
None | None |
Error Codes
Error Code | Description |
---|
None | Required parameter 'name' is missing. |
None | Parameter 'name' is missing or has invalid value. |
None | The programmer with name does not exist. |
Example
The following example pings the programmers 'FP300085' and 'FP30086':
ping_prg -name {FP300085} -name {FP300086}