Description
This Tcl command opens FlashPro Express project (*.pro) that was created in FPExpress.
open_project -project {path and name of the project file} \
[-connect_programmers value]
Arguments
Parameter | Type | Description |
---|
project | string | Specify the path of the FPExpress project with extension *.pro. Project path should include the complete path to the *.pro file. If you do not provide the full path, FlashPro Express infers that you want to open the project from your current working directory. |
connect_programmers | boolean | Valid values are: TRUE, true, 1, FALSE. false or 0. This is optional. Default is 1. |
Return Type | Description |
---|
None | None |
Error Codes
Error Code | Description |
---|
None | Required parameter 'project' is missing. |
Example
This command opens the 'FPPrj1.pro' project from the FPProject1 directory:
open_project -project {./FPProject1/FPPrj1.pro} -connect_programmers 1