17.1.9.1.12 add_include_path
(Ask a Question)Description
Specifies a path to search include files when reading RTL files.
add_include_path <directory>
Arguments
| Parameter | Type | Description |
|---|---|---|
| directory | String | Specifies a path to search include files when reading RTL files. This option is mandatory. |
| Return Type | Description |
|---|---|
| 0 | Command succeeded. |
| 1 | Command failed. There is an error. You can observe the error message in the console. |
List of Errors
| Error Code | Error Message | Description |
|---|---|---|
|
ERR0023 | Required parameter include path is missing. | The directory option is mandatory and must be provided. |
Note: If the directory path is not
correct, then add_include_path will be passed without an error. However,
read_verilog/read_vhd commands will fail due to Verific's
parser.Example
add_include_path component/work/COREABC0/COREABC0_0/rtl/vlog/core