17.1.9.1.1 Working with derive_constraints Utility
(Ask a Question)Derive constraints traverse through the design and allocate new constraints for each instance of component based on previously provided component SDC files. For the CCC reference clocks, it propagates back through the design to find the source of the reference clock. If the source is an I/O, the reference clock constraint will be set on the I/O. If it is a CCC output or another clock source (for example, Transceiver, oscillator), it uses the clock from the other component and reports a warning if the intervals do not match. Derive constraints will also allocate constraints for some macros like on-chip oscillators if you have them in your RTL.
To execute the derive_constraints utility, you must supply a
.tcl file command-line argument with the following information
in the specified order.
- Specify device information using the information in section set_device.
- Specify path to the RTL files using the information in section read_verilog or read_vhdl.
- Set top level module using the information in section set_top_level.
- Specify path to the component SDC files using the information in section read_sdc or read_ndc.
- Execute the files using the information in section derive_constraints.
- Specify path to the SDC derived constraints file using the information in section write_sdc or write_pdc or write_ndc.
Execution and Contents of the derive.tcl File
The following is an example command-line argument to execute the
derive_constraints utility.
$ <libero_installation_path>/bin{64}/derive_constraints derive.tcl
The contents of the derive.tcl file:
# Device information set_device -family PolarFire -die MPF100T -speed -1 # RTL files read_verilog -mode system_verilog project/component/work/txpll0/txpll0_txpll0_0_PF_TX_PLL.v read_verilog -mode system_verilog {project/component/work/txpll0/txpll0.v} read_verilog -mode system_verilog {project/component/work/xcvr0/I_XCVR/xcvr0_I_XCVR_PF_XCVR.v} read_verilog -mode system_verilog {project/component/work/xcvr0/xcvr0.v} read_vhdl -mode vhdl_2008 {project/hdl/xcvr1.vhd} #Component SDC files set_top_level {xcvr1} read_sdc -component {project/component/work/txpll0/txpll0_0/txpll0_txpll0_0_PF_TX_PLL.sdc} read_sdc -component {project/component/work/xcvr0/I_XCVR/xcvr0_I_XCVR_PF_XCVR.sdc} #Use derive_constraint command derive_constraints #SDC/PDC/NDC result files write_sdc {project/constraint/xcvr1_derived_constraints.sdc} write_pdc {project/constraint/fp/xcvr1_derived_constraints.pdc}