21.1.9 Lists and Arrays
(Ask a Question)A list is a way to group data and handle the group as a single entity. To define a list, use curly braces { } and double quotes “ ”. For example, the following set command {1 2 3 }, when followed by the list command, creates a list stored in the variable "a". This list will contain the items "1," "2," and "3".
set a { 1 2 3 }
            Here is another example:
set e 2
set f 3
set a [ list b c d [ expr $e + $f ] ] puts $a
            displays (or outputs):
b c d 5
            Tcl supports many other list-related commands such as lindex,
                linsert, llength, lrange, and
                lappend.
21.1.9.1 Arrays
(Ask a Question)An array is a method to group data. Arrays are collections of items stored in variables. Each item has a unique address that you use to access it. You do not need to declare them or specify their size.
Array elements are managed similarly to other Tcl variables. You create them with the set command, and you can use the dollar sign ($) to access their values.
set myarray(0) "Zero"
set myarray(1) "One"
set myarray(2) "Two"
for {set i 0} {$i < 3} {incr i 1} {\
    puts stdout $myarray($i)}
        Output:
Zero One Two
        In the preceding example, an array called myarray is created using the
                set statement, which assigns a value to its first element. The
            for-loop statement prints out the value stored in each element of the array.
21.1.9.2 Special Arguments (Command-Line Parameters)
(Ask a Question)You can determine the name of the Tcl script file while executing the Tcl script by
            referring to the $argv0 variable.
puts “Executing file $argv0”
            To access other arguments from the command line, you can use the
                lindex command and the argv variable: To read the
            Tcl file name:
lindex $argv 0
            To read the first passed argument:
lindex $argv 1
            For example:
puts "Script name is $argv0" ; # accessing the scriptname puts "first argument is [lindex $argv 0]"
puts "second argument is [lindex $argv 1]" puts "third argument is [lindex $argv 2]" puts "number of argument is [llength $argv]" set des_name [lindex $argv 0]
puts "Design name is $des_name"