21.1.12 Running Tcl Scripts from the Command Line
(Ask a Question)You can run Tcl scripts from your Windows or Linux command line as well as pass arguments to scripts from the command line.
Note: Tcl commands in this section are not case-sensitive.
        To execute a Tcl script file in the Libero SoC Project Manager software from a shell command line:
At the prompt, type the path to the Microchip SoC software installation location followed by the word "SCRIPT" and a colon, and then the name of the script file as follows:
- For Linux: 
<location of Libero SoC software installation>/bin/libero script:<filename>.tcl. For example, to run the Tcl script file "myscript.tcl", type:C:\libero\bin\libero script:myscript.tcl - For Windows: 
<location of Libero SoC software installation>\Designer\bin\libero.exe script:<filename>.tcl. Where<location of Microchip SoC software>is the root directory in which you installed the Microchip SoC software, and<filename>is the name, including a relative or absolute path, of the Tcl script file to execute. For example, to run the Tcl script file "myscript.tcl", type:C:/Microchip/Libero/Designer/bin/libero.exe script:myscript.tcl 
To pass arguments from the command line to your Tcl script file:
At the prompt, type the path to the Microchip SoC software installation location followed by the SCRIPT argument:
- For Linux: <location of
                    Microchip SoC software>\bin\libero “SCRIPT_ARGS:<filename arg1 arg2
                    ...>”. For
                    example:
C:\libero\bin\libero SCRIPT:myscript.tcl “SCRIPT_ARGS:one two three” - For Windows: <location of
                    Microchip SoC software>/Designer/bin/libero.exe “SCRIPT_ARGS:<filename
                    arg1 arg2 ...>”. Where <location of Microchip SoC software> is the root
                    directory in which you installed the Microchip SoC software, and
                    “SCRIPT_ARGS:<filename arg1 arg2 ...>” is the name, including a relative
                    or absolute path, of the Tcl script file and arguments you are passing to the
                    script file. For example:
                    
C:/Microchip/Libero/Designer/bin/libero.exe SCRIPT:myscript.tcl “SCRIPT_ARGS:one two three” 
To obtain the output from the log file:
At the prompt, type the path to the Microchip SoC software installation location followed by the SCRIPT, SCRIPT_ARGS and LOGFILE arguments.
<location of Microchip SoC software> SCRIPT:<filename>.tcl “SCRIPT_ARGS:a b c” LOGFILE:<output.log>
            Where:
location of Microchip SoC softwareis the root directory in which you installed the Microchip SoC software.SCRIPT:<filename>.tclis the name, including a relative or absolute path, of the Tcl script file.SCRIPT_ARGSare the arguments you are passing to the script file.output.logis the name of the log file.
For example:
C:\libero\designer\bin\libero SCRIPT:testTclparam.tcl “SCRIPT_ARGS:a b c” LOGFILE:testTclparam.log