21.1.2 Tcl Command Documentation Conventions
(Ask a Question)The following table lists the typographical conventions used for the Tcl command syntax.
| Syntax Notation | Description | 
|---|---|
command - argument | Commands and arguments appear in Courier New
                            typeface. | 
variable  | Variables appear in Courier New typeface. You
                            must substitute an appropriate value for the variable.  | 
| [-argument value] [variable]+ | Optional arguments begin and end with a square bracket with one exception: if the square bracket is followed by a plus sign (+), then users must specify at least one argument. The plus sign (+) indicates that items within the square brackets can be repeated. Do not enter the plus sign character. | 
# | Comments can be written using a hash (#) sign in the
                            beginning of a text that you want the interpreter to ignore. Comments
                            can be used to provide helping text in your Tcl program. | 
21.1.2.1 Examples
(Ask a Question)Syntax for the get_clocks command followed by a sample command:
get_clocks variable 
            For example, get_clocks clk1.
Syntax for the backannotate command followed by a sample
                        command:
backannotate -name file_name -format format_type -language language -dir directory_name [- netlist] [-pin]
            For example, backannotate -dir {..\design} -name "fanouttest_ba.sdf" -format
                                "SDF" -language "VERILOG" -netlist.
21.1.2.2 Wildcard Characters
(Ask a Question)You can use the following wildcard characters in names used in Tcl commands:
| Wildcard | What it Does | 
|---|---|
\ | Interprets the next character literally. | 
? | Matches any single character. | 
* | Matches any string. | 
[] | Matches any single character among those listed between brackets (that is, [A-Z] matches any single character in the A-to-Z range). | 
A/B12 in the netlist, and you enter that name as
                A\\/B* in a PDC command, you will not be able to find it. In this
            case, you must specify the name as A\\\\/B*.21.1.2.3 Special Characters [ ], { }, and \
(Ask a Question)Sometimes square brackets ([ ]) are part of the command syntax. In these cases, you must either enclose the open and closed square brackets characters with curly brackets ({ }) or precede the open and closed square brackets ([ ]) characters with a backslash (\). If you do not, you will get an error message.
21.1.2.4 Entering Arguments on Separate Lines
(Ask a Question)To enter an argument on a separate line, you must enter a backslash (\) character at the end of the preceding line of the command as shown in the following example:
backannotate -dir \
{..\design} -name "fanouttest_ba.sdf" -format "SDF" -language "VERILOG" \
-netlist