TCPIP_HTTP_NET_ConnectionSocketGet Function
C
NET_PRES_SKT_HANDLE_T TCPIP_HTTP_NET_ConnectionSocketGet(
TCPIP_HTTP_NET_CONN_HANDLE connHandle
);
Description
The function returns the network transport socket of the specified HTTP connection. The user gets access to the connection socket which it can use for debugging or directly sending/reading data.
Preconditions
None.
Parameters
Parameters | Description |
---|---|
connHandle | HTTP connection handle. |
Returns
- NET_PRES_SKT_HANDLE_T for the connection defined by connHandle.
Remarks
This function gives direct access to the underlying transport socket. It is meant for test/advanced usage only. The regular connection functions should be used for manipulation of the connection data. Using the socket directly for data manipulation will disrupt the HTTP server functionality.
Example
uint32_t byteCount;
int sktRxSize;
byteCount = TCPIP_HTTP_NET_ConnectionByteCountGet(connHandle);
sktRxSize = TCPIP_HTTP_NET_ConnectionReadBufferSize(connHandle);
if(byteCount > sktRxSize)
{ // Configuration Failure
TCPIP_HTTP_NET_ConnectionStatusSet(connHandle, TCPIP_HTTP_NET_STAT_REDIRECT);
return TCPIP_HTTP_NET_IO_RES_DONE;
}