TCPIP_HTTP_NET_ConnectionRead Function
C
uint16_t TCPIP_HTTP_NET_ConnectionRead(
TCPIP_HTTP_NET_CONN_HANDLE connHandle,
void * buffer,
uint16_t size
);
Description
This function reads an array of data bytes from the connection RX buffer. The data is removed from the FIFO in the process.
Preconditions
connHandle - a valid HTTP connection.
Parameters
Parameters | Description |
---|---|
connHandle | Connection handle. |
buffer | The pointer to the array to store data that was read. |
size | The number of bytes to read. |
Returns
- The number of bytes read from the socket. If less than len, the connection RX buffer became empty or the underlying socket is not connected.
Remarks
If the supplied buffer is null, the data is simply discarded.