TCPIP_HTTP_NET_ConnectionDataBufferGet Function
C
uint8_t* TCPIP_HTTP_NET_ConnectionDataBufferGet(
TCPIP_HTTP_NET_CONN_HANDLE connHandle
);
Description
This function returns a pointer to the HTTP connection internal data buffer. This gives access to the application to the data that's stored in the HTTP connection buffer.
Preconditions
None.
Parameters
Parameters | Description |
---|---|
connHandle | HTTP connection handle. |
Returns
- A pointer to the connection's general purpose data buffer.
Remarks
None.
Example
template_DynPrint(TCPIP_HTTP_NET_CONN_HANDLE connHandle,
const TCPIP_HTTP_DYN_VAR_DCPT* varDcpt,
const TCPIP_HTTP_NET_USER_CALLBACK* pCBack)
{
const uint8_t *ptr;
ptr = TCPIP_HTTP_NET_ArgGet(TCPIP_HTTP_NET_ConnectionDataBufferGet
(connHandle), (const uint8_t*)"name");
if(ptr == 0)
{
ptr = "not set";
}
else
{
strncpy(myBuffer, ptr, sizeof(myBuffer));
ptr = myBuffer;
}
TCPIP_HTTP_NET_DynamicWrite(varDcpt, ptr, strlen(ptr), false);
}