TCPIP_HTTP_NET_ArgGet Function
C
const uint8_t* TCPIP_HTTP_NET_ArgGet(
const uint8_t* cData,
const uint8_t* cArg
);
Description
This function searches through a data array to find the value associated with a given argument. It can be used to find form field values in data received over GET or POST.
The end of data is assumed to be reached when a null name parameter is encountered. This requires the string to have an even number of null-terminated strings, followed by an additional null terminator.
Preconditions
The data array has a valid series of null terminated name/value pairs.
Parameters
Parameters | Description |
---|---|
cData | The buffer to search. |
cArg | The name of the argument to find. |
Returns
- A pointer to the argument value, or NULL if not found.
Remarks
None.
Example
template_DynPrint(TCPIP_HTTP_NET_CONN_HANDLE connHandle, const TCPIP_HTTP_DYN_VAR_DCPT*
varDcpt, const TCPIP_HTTP_NET_USER_CALLBACK* pCBack)
{
const uint8_t *ptr;
ptr = TCPIP_HTTP_NET_ArgGet(TCPIP_HTTP_NET_ConnectionDataBufferGet(connHandle),
(const uint8_t*)"name");
if(ptr == 0)
{
ptr = "not set";
}
else
{
strncpy(myBuffer, ptr, sizeof(myBuffer));
ptr = myBuffer;
}
TCPIP_HTTP_NET_DynamicWrite(varDcpt, ptr, strlen(ptr), false);
}