TCPIP_HTTP_NET_ConnectionIsAuthorizedGet Function
C
uint8_t TCPIP_HTTP_NET_ConnectionIsAuthorizedGet(
TCPIP_HTTP_NET_CONN_HANDLE connHandle
);
Description
This function returns the authorization status for the current HTTP connection. This is one of the values returned by the template_ConnectionFileAuthenticate() function.
Preconditions
None.
Parameters
Parameters | Description |
---|---|
connHandle | HTTP connection handle. |
Returns
- A uint8_t representing the authorization status.
Remarks
None.
Example
uint8_t isAuth;
isAuth = TCPIP_HTTP_NET_ConnectionIsAuthorizedGet(connHandle);