TCPIP_HTTP_NET_ConnectionFileGet Function
C
SYS_FS_HANDLE TCPIP_HTTP_NET_ConnectionFileGet(
TCPIP_HTTP_NET_CONN_HANDLE connHandle
);
Description
This function returns the handle of the current HTTP connection file.
Preconditions
None.
Parameters
Parameters | Description |
---|---|
connHandle | HTTP connection handle. |
Returns
- Handle to File System file belonging to the connection defined by connHandle.
Remarks
None.
Example
uint8_t myBuff[20];
// Get the file handle and read from that file
SYS_FS_FileRead(myBuff, sizeof(myBuff), TCPIP_HTTP_NET_ConnectionFileGet(connHandle));