TCPIP_HTTP_NET_ActiveConnectionCountGet Function
C
int TCPIP_HTTP_NET_ActiveConnectionCountGet(
int* pOpenCount
);
Description
This function will return the number of active and total opened HTTP connections at the current time.
Preconditions
None.
Parameters
Parameters | Description |
---|---|
pOpenCount | Address to store the number of total HTTP opened connections. Could be NULL if not needed. |
Returns
- The number of active/total connections.
Remarks
The value returned by this function is informational only. The number of active connections changes dynamically.
Example
int nConns;
nConns = TCPIP_HTTP_NET_ActiveConnectionCountGet(0);