TCPIP_IPV6_DefaultRouterGet Function
C
const IPV6_ADDR* TCPIP_IPV6_DefaultRouterGet(
TCPIP_NET_HANDLE netH
);
Description
This function returns the current router address for a specified interface.
Preconditions
The IPv6 stack is initialized and the interface is up and configured.
Parameters
Parameters | Description |
---|---|
netH | The interface for which to return the router address. |
Returns
- Valid IPV6_ADDR pointer - If the interface exists and a valid router address exists.
- 0 - If the interface does not exist and a valid router address does not exist.
Remarks
None.