TCPIP_IPV6_RouterAddressAdd Function
C
bool TCPIP_IPV6_RouterAddressAdd(
TCPIP_NET_HANDLE netH,
IPV6_ADDR * rAddress,
unsigned long validTime,
int flags
);
Description
This function adds a unicast address as a routing address to a specified interface.
Preconditions
rAddress - pointer to a valid IPv6 router address, IPv6 stack initialized, and interface up and configured.
Parameters
Parameters | Description |
---|---|
netH | The interface to which the address is to be added. |
rAddress | The router address to add. |
validTime | The time this entry will be valid, in seconds. If 0, the entry will be valid forever. |
flags | Creation flags (not used for now, should be 0). |
Returns
- True - operation succeeded.
- False - Operation failed (interface not valid, interface still configuring, no memory, etc. ).
Remarks
The validTime parameter is relevant for an existent router on the network. If such router does not exist the stack will eventually discard the entry automatically.