TCPIP_IPV6_Flush Function

C

int TCPIP_IPV6_Flush(
    IPV6_PACKET * pkt
);

Description

This function flushes an IP TX packet. Determines the link-layer address, if necessary and calculates the upper-layer checksum, if necessary.

Preconditions

TCPIP_IPV6_Initialize() should be called. TCPIP_IPV6_InterfaceIsReady should be true.

Parameters

ParametersDescription
ptrPacketThe packet to flush.

Returns

  • 1 - If the packet has been transmitted.
  • 0 - If the packet has been queued.
  • < 0 - If the packet has been discarded for some error.

Remarks

None.