TCPIP_IPV6_Get Function
C
uint8_t TCPIP_IPV6_Get(
TCPIP_MAC_PACKET* pRxPkt,
uint8_t* pData
);
Description
This function is used to read the next byte of data from a packet.
Preconditions
TCPIP_IPV6_Initialize() should be called. TCPIP_IPV6_InterfaceIsReady should be true.
Parameters
Parameters | Description |
---|---|
pRxPkt | The MAC RX packet to read data from. |
pData | Byte data to be read. |
Returns
- 1 - On successful read.
- 0 - No byte is available to read.
Remarks
None.