TCPIP_IPV6_MaxDatagramDataSizeGet Function
C
int TCPIP_IPV6_MaxDatagramDataSizeGet(
TCPIP_NET_HANDLE netH
);
Description
This function is a helper to allow retrieving the MDDS on the specified interface.
Preconditions
TCPIP_IPV6_Initialize() should be called. TCPIP_IPV6_InterfaceIsReady should be true.
Parameters
Parameters | Description |
---|---|
netH | Handle of the interface. |
Returns
- The maximum datagram data size that can be transported on the selected interface.
- 0 - Invalid interface specified.
Remarks
None.