TCPIP_IPV6_DASSourceAddressSelect Function
C
IPV6_ADDR_STRUCT * TCPIP_IPV6_DASSourceAddressSelect(
TCPIP_NET_HANDLE hNetIf,
const IPV6_ADDR * dest,
IPV6_ADDR * requestedSource
);
Description
The IPv6 policy table is used to select the destination address. The destination address selection algorithm takes a list of IPv6 addresses (gPolicyTable) and sorts the linked list. There are eight sorting rules. Starting with the last rule and working to the most important, using a stable sorting algorithm, will produce a sorted list most efficiently. The best average run time we'll get with a stable sort with O(1) memory usage is O(n^2), so we'll use an insertion sort. This will usually be most efficient for small lists (which should be the typical case). If a rule determines a result, then the remaining rules are not relevant and should be ignored.
Preconditions
TCPIP_IPV6_Initialize() is required. TCPIP_IPV6_InterfaceIsReady should be true.
Parameters
Parameters | Description |
---|---|
hNetIf | The given interface. |
dest | The destination address. |
requestedSource | A specified source. |
Returns
IPV6_ADDR *
- Pointer to the selected source address - On Success.
- NULL - On Failure.
Remarks
None.