TCPIP_IPV6_Put Function
C
bool TCPIP_IPV6_Put(
IPV6_PACKET * pkt,
unsigned char v
);
Description
This function writes a character of data to a packet.
Preconditions
TCPIP_IPV6_Initialize() is required. TCPIP_IPV6_InterfaceIsReady should be true.
Parameters
Parameters | Description |
---|---|
pkt | The packet. |
v | The character. |
Returns
- True - If the character was written.
- False - If the character was not written.
Remarks
None.