TCPIP_IPV6_TxPacketAllocate Function
C
IPV6_PACKET * TCPIP_IPV6_TxPacketAllocate(
TCPIP_NET_HANDLE netH,
IPV6_PACKET_ACK_FNC ackFnc,
void* ackParam
);
Description
This function dynamically allocates a packet for transmitting IP protocol data and sets the packet IPv6 protocol for a TX packet.
Preconditions
TCPIP_IPV6_Initialize() should be called. TCPIP_IPV6_InterfaceIsReady should be true.
Parameters
Parameters | Description |
---|---|
netH | Interface of the outgoing packet. |
ackFnc | Function to be called when IP is done with the TX packet (finished transmitting). |
ackParam | Parameter to be used for this callback. This has meaning only for the caller of the TCPIP_IPV6_TxPacketAllocate(). |
Returns
- Pointer to the allocated packet - On success.
- NULL - On failure.
Remarks
None.