TCPIP_TCP_IsConnected Function
C
bool TCPIP_TCP_IsConnected(
TCP_SOCKET hTCP
);
Description
This function determines if a socket has an established connection to a remote node. Call this function after calling TCPIP_TCP_ServerOpen()/TCPIP_TCP_ClientOpen() to determine when the connection is set up and ready for use.
Preconditions
TCP socket should have been opened with TCPIP_TCP_ServerOpen()/TCPIP_TCP_ClientOpen(). hTCP - valid socket.
Parameters
| Parameters | Description |
|---|---|
| hTCP | The socket to check. |
Returns
None.
Remarks
A socket is said to be connected only if it is in one of the states: TCPIP_TCP_STATE_ESTABLISHED, TCPIP_TCP_STATE_FIN_WAIT_1, TCPIP_TCP_STATE_FIN_WAIT_2 or TCPIP_TCP_STATE_CLOSE_WAIT In all of these states the socket can exchange data with the other end of the connection (either full duplex or only TX/RX).
Otherwise the call will return false.