TCPIP_TCP_ArrayGet Function
C
uint16_t TCPIP_TCP_ArrayGet(
TCP_SOCKET hTCP,
uint8_t* buffer,
uint16_t count
);
Description
This function reads an array of data bytes from a TCP socket's RX buffer/FIFO. The data is removed from the FIFO in the process.
Preconditions
TCP is initialized.
Parameters
| Parameters | Description |
|---|---|
| hTCP | The socket from which data is to be read. |
| buffer | Pointer to the array to store data that was read. |
| len | Number of bytes to be read. |
Returns
The number of bytes read from the socket. If less than len, the RX FIFO buffer became empty or the socket is not connected.
Remarks
If the supplied buffer is null, the data is simply discarded.