TCPIP_TCP_ClientOpen Function
C
TCP_SOCKET TCPIP_TCP_ClientOpen(
IP_ADDRESS_TYPE addType,
TCP_PORT remotePort,
IP_MULTI_ADDRESS* remoteAddress
);
Description
Provides a unified method for opening TCP client sockets.
Sockets are created at the TCP module initialization, and can be claimed with this function and freed using TCPIP_TCP_Abort or TCPIP_TCP_Close.
Preconditions
TCP is initialized.
Parameters
| Parameters | Description |
|---|---|
| addType | The type of address being used. Example: IP_ADDRESS_TYPE_IPV4. |
| remotePort | TCP port to connect to. The local port for client sockets will be automatically picked by the TCP module. |
| remoteAddress | The remote address to be used. If 0 then the address is unspecified. |
Returns
INVALID_SOCKET - No sockets of the specified type were available to be opened.
TCP_SOCKET handle - Save this handle and use it when calling all other TCP APIs.
Remarks
IP_ADDRESS_TYPE_ANY is not supported (not a valid type for client open)!
If the remoteAddress != 0 (and the address pointed by remoteAddress != 0) then the socket will immediately initiate a connection to the remote host
If the remoteAddress is unspecified, no connection is initiated. Client socket parameters can be set using TCPIP_TCP_Bind, TCPIP_TCP_RemoteBind, etc. calls and then connection initiated by calling TCPIP_TCP_Connect.
Sockets and user threads protection For efficiency reasons, there is NO PROTECTION for each individual API call except to Open and Close sockets! What it means is that:
the user application should close all its sockets before issuing a stack/if down command The stack manager takes care of the internally used sockets
A socket can NOT be used concurrently from multiple threads! It's ok to pass a socket from one thread to another as long as there's is no access from more than one thread at a time