TCPIP_TCP_Connect Function
C
bool TCPIP_TCP_Connect(
TCP_SOCKET hTCP
);
Description
This function will try to initiate a connection on a client socket that is not connected yet. The client socket should have been created with a call to TCPIP_TCP_ClientOpen having the remoteAddress set to 0.
Preconditions
TCP socket should have been opened with TCPIP_TCP_ServerOpen()/TCPIP_TCP_ClientOpen(). hTCP - valid socket.
Parameters
| Parameters | Description |
|---|---|
| hTCP | Handle to the client socket to connect. |
Returns
True - Indicates success.
False - Indicates failure.
Remarks
The call will fail if the client socket has no remote host specified. Use TCPIP_TCP_RemoteBind() to specify a remote host address for the client socket.