TCPIP_TCP_SocketNetSet Function
C
bool TCPIP_TCP_SocketNetSet(
TCP_SOCKET hTCP,
TCPIP_NET_HANDLE hNet
);
Description
This function sets the network interface for an TCP socket
Preconditions
TCP socket should have been opened with TCPIP_TCP_ClientOpen()/TCPIP_TCP_ServerOpen(). hTCP - valid socket.
Parameters
| Parameters | Description |
|---|---|
| hTCP | The TCP socket. |
| hNet | Interface handle. |
Returns
True - Indicates success.
False - Indicates failure.
Remarks
An invalid hNet can be passed (0) so that the current network interface selection will be cleared.