TCPIP_DHCP_InfoGet Function
C
bool TCPIP_DHCP_InfoGet(
TCPIP_NET_HANDLE hNet,
TCPIP_DHCP_INFO* pDhcpInfo
);
Description
This function returns the current state and lease info of the DHCP client on the specified interface.
Preconditions
DHCP module must be initialized.
Parameters
| Parameters | Description |
|---|---|
| hNet | Interface to query. |
| pDhcpInfo | Storage to return the DHCP info. Could be NULL if not needed. |
Returns
True - If the interface is enabled and exists and the DHCP client service is enabled on that interface and a lease is acquired.
False - Otherwise.
Remarks
None.