TCPIP_DHCP_IsEnabled Function
C
bool TCPIP_DHCP_IsEnabled(
TCPIP_NET_HANDLE hNet
);
Description
This function returns the current state of the DHCP client on the specified interface.
Preconditions
The DHCP module must be initialized.
Parameters
| Parameters | Description |
|---|---|
| hNet | Interface to query. |
Returns
True - If the DHCP client service is enabled on the specified interface.
False - If the DHCP client service is not enabled on the specified interface.
Remarks
None.