TCPIP_DHCP_IsBound Function
C
bool TCPIP_DHCP_IsBound(
TCPIP_NET_HANDLE hNet
);
Description
This functin returns the status of the current IP address lease on the specified interface.
Preconditions
None.
Parameters
| Parameters | Description |
|---|---|
| hNet | Interface to query. |
Returns
True - DHCP client has obtained an IP address lease (and likely other parameters) and these values are currently being used.
False - No IP address is currently leased.
Remarks
None.