DRV_ENC28J60_SetMacCtrlInfo Function
C
void DRV_ENC28J60_SetMacCtrlInfo(SYS_MODULE_OBJ object, TCPIP_MAC_MODULE_CTRL * init);
Returns
None.
Description
ENC28J60 Set MAC Control Information This function is used to pass in the TCPIP_MAC_CONTROL_INIT information that is used for allocation and deallocation of memory, event signaling, etc. This function is needed to be called so that the driver can enter initialization state when the tasks function is called.
Preconditions
The driver had to be successfully initialized with ENC28J60_Initialize.