DRV_ENC28J60_Initialize Function
C
SYS_MODULE_OBJ DRV_ENC28J60_Initialize(SYS_MODULE_INDEX index, SYS_MODULE_INIT * init);
Returns
Valid handle to the driver instance - If successful
SYS_MODULE_OBJ_INVALID - If unsuccessful
Description
ENC28J60 Initialization This function initializes the ENC28J60 Driver with configuration data passed into it by either the system_init function or by the DRV_ENC28J60_StackInitialize function. Calling this function alone is not enough to initialize the driver, DRV_ENC28J60_SetMacCtrlInfo must be called with valid data before the driver is ready to be opened.
Preconditions
None.
Parameters
Parameters | Description |
---|---|
index | This is the index of the driver instance to be initialized. The definition DRV_ENC28J60_NUM_DRV_INSTANCES controls how many instances are available. |
init | This is a pointer to a DRV_ENC28J60_CONFIG structure. |