DRV_ENC28J60_ParametersGet Function

C

TCPIP_MAC_RES DRV_ENC28J60_ParametersGet(DRV_HANDLE hMac, TCPIP_MAC_PARAMETERS* pMacParams); 

Returns

  • TCPIP_MAC_RES_TYPE_ERR - if the hMac is invalid

  • TCPIP_MAC_RES_OK - if the hMac is valid

Description

ENC28J60 Get Parameters Get the parameters of the device, which includes that it is an Ethernet device and what it's MAC address is. Users of the ENC28J60 must generate a unique MAC address for each controller used. The client had to be successfully opened with DRV_ENC28J60_Open.

Parameters

ParametersDescription
hMacthe successfully opened handle
pMacParamspointer to put the parameters