TCPIP_HTTP_CurrentConnectionByteCountGet Function
C
uint32_t TCPIP_HTTP_CurrentConnectionByteCountGet(
HTTP_CONN_HANDLE connHandle
);
Description
This function returns the current value of the counter showing the number of bytes available to be read on the connection.
Preconditions
None.
Parameters
Parameters | Description |
---|---|
connHandle | HTTP connection handle. |
Returns
Current connection byte count, how many bytes have been read so far.
Remarks
None.
Example
switch(TCPIP_HTTP_CurrentConnectionPostSmGet(connHandle))
{
case SM_CFG_SNMP_READ_NAME:
// If all parameters have been read, end
if(TCPIP_HTTP_CurrentConnectionByteCountGet(connHandle) == 0u)
{
return HTTP_IO_DONE;
}
.
.
.
}