TCPIP_HTTP_CurrentConnectionIsAuthorizedSet Function
C
void TCPIP_HTTP_CurrentConnectionIsAuthorizedSet(
HTTP_CONN_HANDLE connHandle,
uint8_t auth
);
Description
This function sets the authorization status for the current HTTP connection. This has to be one of the values in the set returned by the TCPIP_HTTP_FileAuthenticate() function.
Preconditions
None.
Parameters
Parameters | Description |
---|---|
connHandle | HTTP connection handle. |
auth | New authorization state. |
Returns
None.
Remarks
None.
Example
uint8_t auth = 0x80;
TCPIP_HTTP_CurrentConnectionIsAuthorizedSet(connHandle, auth);