TCPIP_HTTP_CurrentConnectionDataBufferSizeGet Function

C

uint16_t TCPIP_HTTP_CurrentConnectionDataBufferSizeGet(
    HTTP_CONN_HANDLE connHandle
);

Description

This function returns the size of the HTTP connection internal data buffer. This buffer is created at the HTTP initialization using the size specified in TCPIP_HTTP_MODULE_CONFIG.dataLen .

Preconditions

None.

Parameters

ParametersDescription
connHandleHTTP connection handle.

Returns

Size of the connection's general purpose data buffer.

Remarks

Currently the size of the buffer is the same for all connections. The connHandle parameter is not used.