TCPIP_HTTP_CurrentConnectionHandleGet Function
C
HTTP_CONN_HANDLE TCPIP_HTTP_CurrentConnectionHandleGet(
int connIx
);
Description
This function will return the connection handle of the requested HTTP connection index.
Preconditions
None.
Parameters
Parameters | Description |
---|---|
connIx | The HTTP connection ix. |
Returns
A valid connection handle if the connection index is valid.
0 if there is no such connection.
Remarks
None.
Example
HTTP_CONN_HANDLE connHandle;
connHandle = TCPIP_HTTP_CurrentConnectionHandleGet(0);