TCPIP_HTTP_SSI_ATTR_DCPT Structure

C

typedef struct {
    const char* attribute;
    char* value;
} TCPIP_HTTP_SSI_ATTR_DCPT;

Description

Data structure: TCPIP_HTTP_SSI_ATTR_DCPT

This data type defines the structure of a SSI command attribute descriptor. When the user registers a template_SSINotification() function for SSI processing, this callback will receive info about the SSI attribute descriptors.

Members

MembersDescription
attributeThe SSI attribute of the command.
valueThe SSI value.

Remarks

The SSI commands consist of pairs of (attribute, value) tokens. For example: < !--#set var="varname" value="varvalue" -- > has 2 pairs: pair 1 - attribute = var value = varname pair 2 - attribute = value value = varvalue