TCPIP_HTTP_NET_ArgGet Function

C

const uint8_t* TCPIP_HTTP_NET_ArgGet(
    const uint8_t* cData, 
    const uint8_t* cArg
);

Description

This function searches through a data array to find the value associated with a given argument. It can be used to find form field values in data received over GET or POST.

The end of data is assumed to be reached when a null name parameter is encountered. This requires the string to have an even number of null-terminated strings, followed by an additional null terminator.

Preconditions

The data array has a valid series of null terminated name/value pairs.

Parameters

ParametersDescription
cDataThe buffer to search.
cArgThe name of the argument to find.

Returns

  • A pointer to the argument value, or NULL if not found.

Remarks

None.

Example

template_DynPrint(TCPIP_HTTP_NET_CONN_HANDLE connHandle, const TCPIP_HTTP_DYN_VAR_DCPT* 
                        varDcpt, const TCPIP_HTTP_NET_USER_CALLBACK* pCBack)
{
    const uint8_t *ptr;

    ptr = TCPIP_HTTP_NET_ArgGet(TCPIP_HTTP_NET_ConnectionDataBufferGet(connHandle), 
                                (const uint8_t*)"name");
    if(ptr == 0)
    {
        ptr = "not set";
    }
    else
    {
        strncpy(myBuffer, ptr, sizeof(myBuffer));
        ptr = myBuffer;
    }

    TCPIP_HTTP_NET_DynamicWrite(varDcpt, ptr, strlen(ptr), false);
        
}