TCPIP_HTTP_NET_DynamicWriteString Function
C
bool TCPIP_HTTP_NET_DynamicWriteString(
const TCPIP_HTTP_DYN_VAR_DCPT* varDcpt,
const char* str,
bool needAck
);
Description
This function takes a 0 terminated ASCII string and sends it to the HTTP connection as part of the HTTP dynamic variable processing.
Preconditions
varDcpt - a valid dynamic variable descriptor.
Parameters
Parameters | Description |
---|---|
varDcpt | Dynamic variable descriptor as passed in the template_DynPrint() function. |
str | The string to be written. |
needAck | If true, once the buffer is processed internally, template_DynAcknowledge() will be called. |
Returns
True - Data buffer has been queued for output.
False - An invalid buffer was provided or the buffer could not be queued because of lack of resources (descriptors).
Remarks
This is just a helper. The actual function called is still TCPIP_HTTP_NET_DynamicWrite(). That means that the supplied string has to be persistent. See the remarks for TCPIP_HTTP_NET_DynamicWrite().