TCPIP_HTTP_NET_ConnectionCallbackPosSet Function

C

void TCPIP_HTTP_NET_ConnectionCallbackPosSet(
    TCPIP_HTTP_NET_CONN_HANDLE connHandle, 
    uint32_t callbackPos
);

Description

This function will set the current value of the callback position indicator for the HTTP connection identified by connHandle. The callback position indicator is used in the processing of the HTTP dynamic variables. When set to a value != 0, it indicates to the HTTP server that the application has more pending processing that needs to be done.

Preconditions

None.

Parameters

ParametersDescription
connHandleHTTP connection handle.
callbackPosNew connection callback position value.

Returns

None.

Remarks

None.