TCPIP_HTTP_NET_ConnectionFileGet Function

C

SYS_FS_HANDLE TCPIP_HTTP_NET_ConnectionFileGet(
    TCPIP_HTTP_NET_CONN_HANDLE connHandle
);

Description

This function returns the handle of the current HTTP connection file.

Preconditions

None.

Parameters

ParametersDescription
connHandleHTTP connection handle.

Returns

  • Handle to File System file belonging to the connection defined by connHandle.

Remarks

None.

Example

uint8_t myBuff[20];

// Get the file handle and read from that file
SYS_FS_FileRead(myBuff, sizeof(myBuff), TCPIP_HTTP_NET_ConnectionFileGet(connHandle));