9.2.22 --library-path
dir (-L dir)
Add dir to library
search path.
Add path dir to the list of paths that
xc-dsc-ld will search for
archive libraries and xc-dsc-ld control scripts. You may use this option any number of times. The
directories are searched in the order in which they are specified on the command line. All
-L options apply to all -l options, regardless of the order in which the options appear. The library
paths can also be specified in a link script with the SEARCH_DIR command. Directories specified this way are searched at the point
in which the linker script appears in the command line.