3.6 LEDs
The WFI32-IoT 2.0 on-board LEDs are categorized into three types:
- Power LEDs
- PKOB4 LEDs
- LEDs related to the WFI32E03PC module:
The following table lists the LEDs that can be turned ON or OFF using the connected GPIO pins.
The WFI32-IoT 2.0 on-board LEDs are categorized into three types:
The following table lists the LEDs that can be turned ON or OFF using the connected GPIO pins.