Input Mode 10: Stop Output on Edge, Maintain Frequency
In Input mode 10 the input event will cause the corresponding output to stop as long as the input is active. If the input goes low while there should have been an on time on the corresponding output, the output will be deactivated for the rest of the on time, too. The TCD counter is not affected by the event, only the output.
If Input mode 10 is used on input A and an input event occurs, the WOA will be OFF as long as the event lasts. If released during an on time, it will be OFF for the rest of the on time.
If Input mode 10 is used on input B and an input event occurs, the WOB will be OFF as long as the event lasts. If released during an on time, it will be OFF for the rest of the on time.