Input Mode 5: Stop all Outputs, Execute Dead Time while Fault Active
When Input mode 5 is used, both input A and input B give the same functionality:
The input event stops the outputs and starts on the opposite dead time if it occurs during an on time. If the event occurs during a dead time, it will continue until the next on time should start, but instead, it will jump to the next dead time. As long as the input event is active, alternating dead times will occur. When the input event stops, the ongoing dead time will finish and the next on time will continue in the normal flow.