Input Mode 9: Stop Output at Level, Maintain Frequency

In Input mode 9 a positive edge on the input event while the corresponding output is on will cause the output to stop during the rest of the on time. The TCD counter will not be affected by the event, only the output.

If Input mode 9 is used on input A and a positive input event occurs while in On time A, the output will be OFF for the rest of the on time.

Figure 23-22. Input Mode 9 on Input A

If Input mode 9 is used on input B and a positive input event occurs while in On time B, the output will be OFF for the rest of the on time.

Figure 23-23. Input Mode 9 on Input B