Input Mode 2: Stop Output, Execute Opposite Compare Cycle, and Wait
An input Event in Input mode 2 will stop the output signal, execute to the opposite dead time and on time, then wait until the input event goes low before the TCD counter continues. If the input is done before the opposite dead time and on time have finished, there will be no waiting, but the opposite dead time and on time will continue.
If Input mode 2 is used on input A, an event will only have an effect if the TCD is in Dead-time A or On time A, and it will only affect the output WOA.
If Input mode 2 is used on input B, an event will only have an effect if the TCD is in Dead-time B or On time B, and it will only affect the output WOB.